Technical FAQs

Ask a Question

How to auto enable the LXM32 drive using SoMove?

Issue:
Auto enable the LXM32 drive using SoMove

Product Line:
LXM32

Resolution:
Instead of having to activate an input in order to enable the LXM32 drive, you can set the following parameters to automatically enable the drive on power-up:
In SoMove (See attached):
Axis Configuration > IO_AutoEnaConfig = ON
Axis Configuration > IO_AutoEnable = AutoOn
Was this helpful?
What can we do to improve the information ?