Browse FAQs

Where is the Modbus Map located and how is the Modbus protocol set for ION Meters?

Published date: 31 July 2019

Issue
A user would like to read values from an ION meter via Modbus register reads. 

Product Line
ION 7300, 7500, 7600, 7550, 7650, 8300, 8400, 8500, 8600, 8650 series meters

Environment
Modbus register list

Resolution
Attached is the default register map for the following meters: ION 7300, 7500, 7600, 7550, 7650, 8300, 8400, 8500, 8600, 8650. Please note that this is a default map only and can be modified using the ION programming environment on-board the meter. For additional information on modifying the default modbus registers, please see the attached Modbus and ION Technology document. 

For specific instructions on how to read energy values, refer to KB FA233789

For the modbus maps for the PM8000 and ION7400 series meters, refer to KB FA244203

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.