Browse FAQs

What is the HTS Code, ECCN, and Country of origin for the HMISTU855?

Published date: 12 August 2019

Issue:
When shipping the HMISTU855 to locations outside of the United States and Canada, it is often necessary to provide the HTS Code, ECCN Number, and the country of origin to the border authorities. 

Product Line:
HMISTU, HMIS5T, HMISTU855, HMISTU655

Resolution:
The HTS Code is 8537108000.
 
The ECCN Number is EAR99.
 
The Country of Origin is China (CN).

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.