Browse FAQs

Can a 63.75" tall PDU be installed into a 38U NetShelter CX cabinet?

Published date: 05 August 2019

Issue:
The 63.75" tall PDU does not fit onto the accessory rail. Will it fit anywhere else inside the cabinet? 

Product Line: 
NetShelter CX 

Environment: 
AR4038A, AR4038IA

Cause:
One of the 63.75" tall PDUs has been specc'd into a 38U NetShelter CX cabinet. 

Resolution:
Yes, the 63.75" tall PDUs can attach to the rear mounting rail. Please see the attached file for mounting instructions. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.