Technical FAQs

Ask a Question

What is the difference between IFE and EIFE module?

To compare EIFE with IFE - 

Embedded Webpages Yes Yes
Cradle management (CE, CD, CT) Yes Yes
Daisy chain capability Yes Yes
Space 72 x 105 x 71 mm 0 additional space in swb
Power supply Thru ULP 24V DC

Was this helpful?
What can we do to improve the information ?