Technical FAQs

Ask a Question

How MTZ can be integrated to a Modbus Serial Line architecture?

It will not be possible, only Modbus TCP will be available through Embedded IFE module for Wave M.
NB: A solution to add a Modbus SL connection is on working and should be available in next waves.
Was this helpful?
What can we do to improve the information ?