Search FAQs
Is it possible to compare or convert configurations from ATV61/71 to ATV600 series in SoMove?
Issue:
Can you convert configurations from ATV61/71 to Process ATV600 in SoMove?
Product Line:
Altivar 61, Altivar 71 , Altivar 630, Altivar 650
Environment:
All
Cause:
SoMove Software
Resolution:
SoMove does not have the capability to compare or convert configurations between ATV61/71 and ATV600 series Process drives.
Can you convert configurations from ATV61/71 to Process ATV600 in SoMove?
Product Line:
Altivar 61, Altivar 71 , Altivar 630, Altivar 650
Environment:
All
Cause:
SoMove Software
Resolution:
SoMove does not have the capability to compare or convert configurations between ATV61/71 and ATV600 series Process drives.
Released for:Schneider Electric UK
Explore more
Explore more