Browse FAQs

What is the maximum motor lead length you can run the ATV320 drive without a load reactor?

Published date: 05 July 2019

Issue:
What is the max cable length you can run the ATV320 drive without a load reactor?

Product Line:
Altivar 320

Environment:
All

Cause:
Motor cable length distance without a load reactor. 

Resolution:
The ATV320 drive can run up to 164 feet without load reactor.  
You can go up to 328 feet with shielded cable or up to 656 feet with an unshielded cable.
See the table in the attachment.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.