Technical FAQs

Ask a Question

How to define the reference for IKQ Single Phase distribution boards?

In the IKQ catalogue see section 1 which is attached as a PDF to this F.A.Q please see page 5 In this section of the SE8386 you will find the part numbers and descriptions of the distribution boards to which we offer. Explained below is how to work out single phase boards, for three phase boards please see FAQ FA289245

1) Single Phase boards: How to work out the part number? All boards will start with the Reference (SE) followed by (125)Amps then (A) for A type board single phase, then followed by the ways (12) etc which go from 4,6,8,12,16,18 to 24 max

Examples: SE125A6 - 6 Way 125A A board

SE125A8 - 8 Way 125A A Board

SE125A12 - 12 Way 125A A board

SE125A16 - 16 Way 125A A board

SE125A24 - 24 Way 125A A Board



Was this helpful?
What can we do to improve the information ?