Browse FAQs

ATV61: Why can the Forced Local parameter not be change from NO?

Published date: 26 July 2019

Issue:
ATV61: Forced Local parameter not be change from NO

Product line:
ATV61, ATV71, Altivar 61, Altivar 71

Environment:
All

Cause:
Customer wants to use Forced Local but the drive will not allow the change.


Resolution:
Forced local is not compatible with the Profile set to IO.  To use the Forced Local function, the Profile needs to be set to Separate or Not Separate. 

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.