Technical FAQs

Ask a Question

Which breakers are used in the Powerpact 4 MGP style breakers ?

The Powerpact 4 MGP style breakers consist of a NSX breaker with a factort fitted adaptor kit.
The part numbers for these breakers start with MGP and are availabl in 1 to 4 pole devices from 16A to 630A
MGB Example of a Moulded case circuit breaker for use in the Powerpact 4 panelboards
Was this helpful?
What can we do to improve the information ?