Technical FAQs

Ask a Question

Do Schneider Electric offer a 3 phase RCBO in the iC60 range?

Yes this can be achieved using a 3 pole iC60 breaker and then choose a vigi unit A9V02763 for 30mA or A9V06763 for 300mA and attaching these two together.  When the two devices are combined to form the RCBO it will measure 6 mods ( 6 x 18mm) wide.

Image od an iC60 and Vigi unit together to forman RCBO
Was this helpful?
What can we do to improve the information ?