Technical FAQs

Ask a Question

Can the Acti 9 incomer switch SEA9NI1603 have a Undervolt or Shunt fitted

No the SEA9NI1603 CANNOT have a Undervolt or Shunt fitted.

With one exception none of the Switched disconnectors for the B Type boards can have Undervolt trip unit, Shunt trip unit, or Auxiliaries fitted. This is because they are based on the Interpact INS range.
The only Acti9 switch incomer that can have a Undervolt or Shunt or auxilliary fitted is the SEA9NI2254 as this is based on the NSX range
 
Switched Disconnector
for B type boards
Possible
Undervolt
Shunt Trip
Auxiliary
SEA91253N No
SEA91254 No
SEA9NI1603 No
SEA9NI1604 No
SEA9NI2003 No
SEA9N2004 No
SEA9N2254 Yes
SEA9NI2503 No
SEA9NI2504 No

 
Was this helpful?
What can we do to improve the information ?