Technical FAQs

Ask a Question

Do we require a additional adapters for remote display on a PM8000 series meters?

To mount the display remotely you do not need additional equipment or adaptors, the display plugs direct in to meter using the 3m cable

The display is mounted in a 92 x 92mm appature.

Below is a picture showing the Screen, Cable and Controller

PM8000 Remote mounting of screen with 3m cable
 
Was this helpful?
What can we do to improve the information ?