Technical FAQs

Ask a Question

What is the substitution for the GNS safety modules?

Unfortunately there is no direct replacement for the GNS safety relay.
The GNS product was a 115V AC detector amp XPSNS3440 (115VAC) modules. They allowed interfacing and amplifying signals emitted by detectors (2-wire, 3-wire PNP, 3-wire NPN, magnetic detectors or position switches).

They are partially substitutable by the XPSAK351144 (120VAC) or XPSAK371144 (230VAC) for monitoring of 2 inductive sensors (PNP-NPN with short-circuit detection or PNP-PNP without short-circuit detection)
Was this helpful?
What can we do to improve the information ?