Search FAQs
To what standards do the A class and B class filters correspond in the variable speed drives?
EMC environment and EMC input filter Industrial and commercial EMC environments are described by standards, and Schneider Electric has designed EMC filters to comply with the radio interference levels specified in these standards.
Class A and class B filters
Class A filters are mainly used in industrial environments as they are suitable for the EMC environments described by the typical standards for this type of environment:
EN55011 class A group 1 or IEC/EN 61800-3 category C2
EN55011 class A group 2 or IEC/EN 61800-3 category C3
Class B filters are used in commercial (building) or domestic environments as they are suitable for the EMC environments described by the typical standards for these types of environment:
EN55011 class B group 2 or IEC/EN 61800-3 category C1
Class B filters provide higher performance than Class A filters because commercial environments (offices, administration) need to have a higher level of protection than industrial environments.
Schneider Electric offer
The Schneider Electric offer comprises drives with or without filter. If they have a filter, it may be class A or class B.
As an EMC filter incurs expenditure, it is must be optimized by answering the following questions:
However, the complete products are suitable for the majority of cases.
ATV212
Class A and class B filters
Class A filters are mainly used in industrial environments as they are suitable for the EMC environments described by the typical standards for this type of environment:
EN55011 class A group 1 or IEC/EN 61800-3 category C2
EN55011 class A group 2 or IEC/EN 61800-3 category C3
Class B filters are used in commercial (building) or domestic environments as they are suitable for the EMC environments described by the typical standards for these types of environment:
EN55011 class B group 2 or IEC/EN 61800-3 category C1
Class B filters provide higher performance than Class A filters because commercial environments (offices, administration) need to have a higher level of protection than industrial environments.
Schneider Electric offer
The Schneider Electric offer comprises drives with or without filter. If they have a filter, it may be class A or class B.
As an EMC filter incurs expenditure, it is must be optimized by answering the following questions:
- Industrial or commercial environment (most important criterion)
- Distance between drive and motor
- Switching frequency
However, the complete products are suitable for the majority of cases.
ATV212
- ATV212H075M3X to ATV212HD30M3X: without EMC filter
- ATV212H075N4 to ATV212HD75N4: with integrated class A filter
- ATV212W075N4 to ATV212WD75N4: with integrated class A filter
- ATV212W075N4C to ATV212WD75N4C: with integrated class B filter
- ATV312H018M2 to ATV312HU22M2: with integrated class A group 1 filter
- ATV312H037N4 to ATV312HU40N4: with integrated class A group 1 filter
- ATV31HU22M2: with integrated class A group 2 filter
- ATV312HU55N4 to ATV312HD15N4: with integrated class A group 2 filter
- ATV312H018M3 to ATV312HD15M3: without EMC filter
- ATV32 ATV32H018M2 to ATV32HU22M2: with integrated class A group 1 filter
- ATV32H037N4 to ATV32HD15N4: with integrated class A group 1 filter
- ATV12xxxxF1, ATV12H018M3, ATV12x037M3 to ATV12xU22M3: without EMC filter
- ATV12xxxxM2: with class A or class B filter depending on the cable length or switching frequency. Remember they are high-performance.
- ATV61H075M3 to ATV61HU22M3: with integrated class A group 1 filter
- ATV61HU30M3 to ATV61HU75M3: with integrated class A group 2 filter
- ATV61HD11M3X to ATV61HD90M3X: without integrated EMC filter
- ATV61H075N4 to ATV61HU40N4: with integrated class A group 1 filter
- ATV61HU30Y to ATV61HC80Y: with integrated class A group 2 filter
- ATV61W075N4 to ATV61WD90N4: with integrated class A group 1 filter
- ATV61W075N4C to ATV61WD90N4C: with integrated class B filter
- ATV71H037M3 to ATV71HU22M3: with integrated class A group 1 filter
- ATV71HU30M3 to ATV71HU75M3: with integrated class A group 2 filter
- ATV71HD11M3X to ATV71HD75M3X: without integrated EMC filter
- ATV71H075N4 to ATV71HU40N4: with integrated class A group 1 filter
- ATV71HU55N4 to ATV71HC50N4: with integrated class A group 2 filter
- ATV71W075N4 to ATV71WU40N4: with integrated class A group 1 filter
- ATV71WU55N4 to ATV71WD75N4: with integrated class A group 2 filter
- ATV71PU15N4Z to ATV71PU40N4Z: with integrated class A group 1 filter
- ATV71PU55N4Z to ATV71PD11N4Z: with integrated class A group 2 filter
- ATV630U07N4 to ATV630D45N4 with integrated class A group 1 filter
- ATV630D55N4 to ATV630C16N4 with integrated class A group 2 filter,
- ATV930U07N4 to ATV930D45N4 drive have a class A group 1 filter fitted
- ATV930D55N4 to ATV930C16N4 drive has the class A group 2 filter built in a standard.
- ATV950U07N4 to the ATV950D45N4 drive has the Class A group 1 filter
- ATV950D55N4 to the ATV950D90N4 drive has the Class A group 2 filter fitted as standard.
Released for:Schneider Electric UK
Explore more