Technical FAQs

Ask a Question

What is accuracy of the Rogowski CT's used in the NW breakers?

The accuracy is not given only for the CT but for the trip unit asociated with the CT : the value announce is 1.5% for Masterpact and micrologic 5.0P, or Micrologic 5.0E for current measuring.

We refer to the standard IEC 61557-12.

Masterpact NW Air Circuit Breaker
Was this helpful?
What can we do to improve the information ?