Search FAQs
What faults are not protected by Fault Inhibition on the ATV61 drive?
Issue:
What faults are not protected by Fault Inhibition on the ATV61 drive?
Product line:
ATV61, altivar 61
Environment:
all
Cause:
Customer was using Fault Inhibition, but the drive still tripped on SCF5, motor short circuit.
Resolution:
The fault inhibition function will be able to inhibit (not display) the fault detection on the « software » fault.
For the critical, internal or hardware faults, the inhibition function does not work to protect the drive from damage.
The fault list given in the programming manual are the ones that Inhibition will work
All the other critical, internal and hardware faults (SCFx, ILx, INFE, CRFx...) will be always active even with INH (fault inhibition) turned on.
What faults are not protected by Fault Inhibition on the ATV61 drive?
Product line:
ATV61, altivar 61
Environment:
all
Cause:
Customer was using Fault Inhibition, but the drive still tripped on SCF5, motor short circuit.
Resolution:
The fault inhibition function will be able to inhibit (not display) the fault detection on the « software » fault.
For the critical, internal or hardware faults, the inhibition function does not work to protect the drive from damage.
The fault list given in the programming manual are the ones that Inhibition will work
- EnF, InFA, InFb, SOF, SPF, and tnF, APF, CnF, COF, EPF1, EPF2, FCF2, Fd1, LFF2, LFF3, LFF4, nFF, ObF, OHF, OLC, OLF, OPF1, OPF2, OSF, OtF1, OtF2, OtFL, PHF, PtF1, PtF2, PtFL, SLF1, SLF2, SLF3, SPIF, SSF, tJF, ULF and USF faults can be inhibited and cleared remotely by means of a logic input or control bit ([Fault inhibit assign.] (InH) parameter
All the other critical, internal and hardware faults (SCFx, ILx, INFE, CRFx...) will be always active even with INH (fault inhibition) turned on.
Released for:Schneider Electric UK
Explore more
Range:
Explore more
Range: