Search FAQs
What is the part number for the ATS48 remote keypad display mounting kit, and what is included in it?
Issue:
Is there a remote keypad for the ATS48?
Product Line:
ATS48
Environment:
All
Cause:
Remote keypad required
Resolution:
Part number VW3G48101 is the kit, and includes:
Keypad with 3–character 7–segment display,
IP65 cover and seal,
Mounting screws,
3 meter cable to connect keypad display to Altistart 48.
Note: The kit is not rated for outdoor use.
Is there a remote keypad for the ATS48?
Product Line:
ATS48
Environment:
All
Cause:
Remote keypad required
Resolution:
Part number VW3G48101 is the kit, and includes:
Keypad with 3–character 7–segment display,
IP65 cover and seal,
Mounting screws,
3 meter cable to connect keypad display to Altistart 48.
Note: The kit is not rated for outdoor use.
Released for:Schneider Electric UK
Explore more
Range:
Explore more
Range: