Search FAQs
What is the maximum current rating of an ATS22 relay?
Issue:
Maximum current rating of an ATS22 relay.
Product Line:
Altistart 22, ATS22
Environment:
All
Cause:
N/A
Resolution:
Max switching capability:
5A - 250VAC or 30VDC on resistive load (p.f.=1)
2A - 250VAC or 30VDC on inductive load (p.f=0.4)
Maximum current rating of an ATS22 relay.
Product Line:
Altistart 22, ATS22
Environment:
All
Cause:
N/A
Resolution:
Max switching capability:
5A - 250VAC or 30VDC on resistive load (p.f.=1)
2A - 250VAC or 30VDC on inductive load (p.f=0.4)
Released for:Schneider Electric UK
Explore more
Range:
Explore more
Range: