Technical FAQs

Ask a Question

Can the trip units be set between settings?

The NSX thermal magnetic trips can only be set at the incrament settigs provided, they cannot be set mid way between points.

This is true for all the ranges of the Micrologic Trip units

Micrologic range from 2.2 to 7.2
Was this helpful?
What can we do to improve the information ?