Browse FAQs

Will an External Fault triggered by a logic input be recorded in the fault history on an ATV61 / ATV71 series drive?

Published date: 30 July 2019

Issue:
Will an External Fault triggered by a logic input be recorded in the fault history on an ATV61 / ATV71 series drive?  
 
Product Line:
ATV61 / ATV71 series drives
 
Environment
All models, All serial numbers
 
Cause
Customer needs a fault history on how many times an external fault is triggered.
 
Resolution:
An external fault, triggered by a logic input, will be recorded into the fault history and can be retrieved by navigating to the diagnostics menu and entering the fault history sub-menu.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.