Browse FAQs

What is the max current rating on the ATV61 and ATV71 drives 10vdc power supply?

Published date: 30 July 2019

Issue:
What is the max current rating on the ATV61 and ATV71 drives 10vdc power supply?

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Needs to connect some small LEDs using the 10vdc supply so they need to know the max current current ratings.

Resolution:
The max current rating  is 10mA max @ 10vdc.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.