Technical FAQs

Ask a Question

What size cable is a SEA91254/SEA91253N capable of handling?

Both of these incomers can handle upto 50mm2 cable. If you have a larger cable then you will need to order an incomer greater than 125amps.
Note: Spreaders are not available for this size incomer.
SEA91254 Four pole incomer 125A
Was this helpful?
What can we do to improve the information ?