Browse FAQs

What is the maximum roof load rating for NetShelter SX and SV cabinets?

Published date: 05 August 2019

Issue:
Information regarding the maximum load rating for the roof is required

Product Line:
NetShelter SX, NetShelter SV

Environment:
All versions and serial ranges.

Cause:
The load rating should not be exceeded.

Resolution:
The roofs of both the NetShelter SX and SV cabinets are rated to 200 lbs.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.