Browse FAQs

What is the efficiency of ATV71 drives?

Published date: 13 August 2019

Issue:
What is the efficiency of ATV71 drives?

Product Line:
ATV71 drives

Environment:
All ATV71 drives

Cause:
Efficiency on ATV71 drives

Resolution:
The efficiency varies by (part number) at 100% load.  
The lowest is 88.9% for the 0.5 HP 230V unit.
All others are above 91% with the majority exceeding 97%

At less than 100% load, the efficiency will decrease.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.