Browse FAQs

Does the keypad VW3A1101 come standard with the ATV61 or ATV71 drive?

Published date: 30 July 2019

Issue:
Does the keypad VW3A1101 come standard with the ATV61 or ATV71 drive?

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Wants to know if the graphics keypad will come with the drive when you order it.

Resolution:
Yes the keypad comes with the ATV61 or ATV71 drive when you order the drive.   If you add the suffix letter Z it will delete the keypad when ordering the drive.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.