Browse FAQs

Are there any screen protective sheets for the Magelis HMIGTU panels?

Published date: 12 August 2019

Issue
I would like to protect my HMIGTU series screen against dirt, UV, or harsh environments, what protective sheets are available?

Product Line
Magelis HMIGTU

Environment
Physical HMI

Resolution
There are three types of screen protection devices for the HMIGTU series:

Dirt-resistant sheets (comes in a box of 5):
HMIZG63………………for HMIDT351 (7" Wide)
HMIZD65W…………....for HMIDT551 (10" Wide)
HMIZD66W…………....for HMIDT651 (12" Wide)
HMIZG65………………for HMIDT542 (10.4")
HMIZG66………………for HMIDT642 (12.1")
MPCYK50SPSKIT.…...for HMIDT732 (15")

UV Protective sheets (comes in a box of 5):
HMIZUV3W….……….for HMIDT351 (7" Wide)
HMIZUV5W….……….for HMIDT551 (10" Wide)
HMIZUV6W….……….for HMIDT551 (12" Wide)
HMIZUV5……………..for HMIDT542 (10.4")
HMIZUV6…....………..for HMIDT642 (12.1")
HMIZUV7……………..for HMIDT732 (15")

Plastic Covers for Harsh Environment (IP67):
HMIZDCOV5………….for HMIDT542 (10.4")
HMIDZCOV6………….for HMIDT642 (12.1")
HMIDZCOV7………….for HMIDT732 (15")

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.