Technical FAQs

Ask a Question

What is the highest rated iLine (Square D) panel board?

The iLine panel boards (Square D by Schneider Electric) go up to 630 Amps, i-Line MCCB panelboards Size 2 630A.

I-Line MCCB panelboards Size 2 630A
For higher Amperage then Powerpact 4 board are required
Was this helpful?
What can we do to improve the information ?