Technical FAQs

Ask a Question

Is it possible to monitor the status of NSX switch over modbus?

Yes it is possible, you will need a low voltage OF (29452) connected to a smartlink modbus (A9XMSB11).

The smartlink bus gives the user up to 11 digital input / output channels and is designed to connect over Modbus.
Was this helpful?
What can we do to improve the information ?