Technical FAQs

Ask a Question

Are preset speeds active on the ATV212 when in local control?

Issue:
Are preset speeds active on the ATV212 when in local control?

Product Line:
ALTIVAR 212

Environment:
All serial number

Cause:
N/A

Resolution
No, preset speeds are not active when in local control.
Was this helpful?
What can we do to improve the information ?