Technical FAQs

Ask a Question

What is the Logic Instruction Capacity In PICED?

The PICED software is the programming interface for C-Bus embedded devices.
The PICED software is the programming interface for CBUS
The Logic Instruction Capacity In PICED is used to allow more than the recommended instructions in the logic engine.

The maximum amount of instructions can be increased within the Logic engine by going to Tools -> Logic Options -> Errors tab.

This is also generally a sign though that the amount of logic on the unit is reaching its capacity

 
Was this helpful?
What can we do to improve the information ?