Browse FAQs

Changing time format in PICED from 12 to 24Hour

Published date: 01 August 2019

This option can be configured on the Tools page of the unit under Region/Language -> Regional Options tab -> Customize -> Time tab.

From here you will be able to select HH:mm:ss from the Time format drop down menu which should display the time on the touchscreen as desired

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.