Technical FAQs

Ask a Question

NSX Single pole terminal shield LV429320 is in catalogue but not on system?

Unfortunately there is an error in the Ready to Install catalogue SE8863 JAN 2015 on page 8/18.

The part number LV429320 is incorrect

The correct part number should be LV438320 (Pair of single pole terminal shields)
Was this helpful?
What can we do to improve the information ?