Technical FAQs

Ask a Question

CBUS: PCI found error - failed to Identify Project name and no Cbus network in view on tool kit.


This problem will be caused by Two or more burdons on the system, Hardware and software burdons were enabled.
Solution: Track through the network and find the Unit that has the software burdon enabled in the global settings, then switch this off and also remove hardware burdon (if applicable) then then restart toolkit and load up project this will solve this issue
Was this helpful?
What can we do to improve the information ?