Browse FAQs

What are possible causes for the ATS48 softstart to trip the breaker?

Published date: 05 August 2019

Issue:
What are possible causes for the ATS48 softstart to trip the Main breaker?

Product Line:
ATS48, Altistart 48

Environment:
All models and serial numbers

Cause:
Possible causes:
1.  The load is excessive
2.  Shorted SCR
3.  Shorting contactor is welded in the closed position
4. Incorrect settings on the breaker

Resolution:
If excessive load, may need to upsize the motor and soft start.  Try increasing the acceleration time.  Decrease the load.
With the soft start powered down, perform static checks on the SCR's. If shorted SCR's, repair or replace.
If shorting contactor is welded, replace the shorting contactor.
Check SCRS of the softstart.  This can be done by following FAQ listed here: 
https://www.schneider-electric.us/en/faqs/FA221890/
Dial proper trip settings on the breaker if present.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.