Browse FAQs

Are the VW3A1101 stored files lost if the HMI is disconnected from a drive?

Published date: 30 July 2019

Issue:
Are the VW3A1101 stored files lost if the HMI is disconnected from a drive?

Product Line:
ATV61  ATV71

Environment:
All

Cause:
Would like to transfer files

Resolution:
No.  The files that are stored in the HMI remain intact when the HMI is disconnected from the drive.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.