Browse FAQs

Where can I get the pinout for the RJ45 modbus port on the ATS22?

Published date: 01 July 2019

Issue:
Where can I get the pin out for the RJ45 modbus port on the ATS22?

Product Line:
Altistart 22

Environment:
All serial numbers

Cause:
Modbus RJ45 pinout

Resolution:
RJ45 Pin 4 = D1 : RJ45 Pin 5 = D0 : RJ45 Pin 8 Common; See the ATV22 user manual wiring control terminals for a complete listing

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.