Browse FAQs

How do I change the default display to show PSI on the keypad of the ATV61 or ATV71 drive?

Published date: 30 July 2019

Issue:
Display custom "User Name"

Product Line:
ATV61 and ATV71

Environment:
All models and serial numbers

Cause:
None

Resolution:
How to customize your display to show your [User Name] as PSI using the PID Feedback
  1. Scale the AI2 to 0-20mA
    1. From the drive menu go to 1.5 [INPUTS / OUTPUTS CFG] press enter
    2. Go to AI2 CONFIGURATION press enter
    3. Set AI2 Min. Value to 0
    4. Set AI2 Max. Value to 20
  2. From the MAIN menu go to Menu 7 – [DISPLAY CONFIG]
    1. Select Sub-menu 7.1 – [USER PARAMETERS]
    2. Go to [PARAMETER SELECTION]
    3. Go to sub-menu 1.2 [MONITORING]
    4. Select [PID feedback] (a checkmark will appear in the box)
    5. Press the (ESC) button 2 times
  3. Go to [CUSTOMIZED SELECTION]
    1. Select [PID feedback]
    2. Select [User name]
    3. Rename the parameter using the thumbwheel
      1. Turn the thumbwheel clockwise to “P” then press “F3”
      2. Turn the thumbwheel again to “S” then press “F3”
      3. Turn the thumbwheel again to “I” then press “ENTER”
    4. Press (ESC) back to the main menu.
    5. Go to Menu 6. [MONITORING CONFIG.].  Press “ENTER”
    6. Go to [MONITOR SCREEN TYPE].  Press “ENTER”
    7. Go to [PARAMETER SELECTION].  Press “ENTER”
    8. Scroll down to the newly named parameter “PSI”, Press “ENTER”
    9. Press the (ESC) button
    10. Multiplier = 100
    11. Divisor = 16
    12. Press the ESC button until the display shows “PSI”
  4. Make the your [User name] as the default display
    1. Enter menu 6. [MONITORING CONFIG] from the MAIN MENU
    2. Enter menu 6.2 [MONITOR SCREEN TYPE]
    3. Enter [PARAMETER SELECTION]
    4. Select your [User name] parameter from the list of parameters (Note:  a maximum of two parameters is allowed.  You may need to unselect a parameter in order to select your [User name]”
    5. Press ESC 4 times to see your [User name] displayed on the HMI.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.