Browse FAQs

How can I configure communication between a Twido Port 499TWD01100 and an XBTGT?

Published date: 01 August 2019

The TwidoPort 499TWD01100 module is an Ethernet/Modbus RTU interface designed for Twido Version 3.0, compact or modular.  For the following parameters, refer to the extra info. below: Setting 499TWD01100 interface parameters in Twido Suite, Setting 499TWD01100 interface parameters in Vijeo Designer, Setting XBTGT parameters in Vijeo Designer  Note: In the Vijeo Designer configuration window, the unit's ID should be at 1 (@modbus of the 499TWD interface) instead of the default value (255)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.