How can I see the last faults that occurred on an ATV61 or ATV71 drive?
Issue:
Wants to see the last faults that occurred on an ATV61 or ATV71 drive.
Product Line:
ALTIVAR 71 ATV71 ATV61 Altivar 61
Environment:
All
Cause:
Faults
Resolution:
Go to menu 1.10 Diagnostics then to Fault History.
Faults are listed most recent to oldest.
You can highlight and press enter on each fault to confirm a number of things that registered at the time of fault.