Technical FAQs

Ask a Question

Are 23" mounting rails available for NetShelter SX cabinets?

Issue: 
Some equipment requires 23 inch wide mounting rails.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
A customer has 23 inch wide equipment and wants to mount it into a NetShelter SX cabinet.

Resolution: 

All 42U and 48U NetShelter SX 750 mm (30") wide cabinets are available with 23" mounting rails installed. These cabinets are not in stock, but they can be built to order.
  • For customers who already own a 42U 750mm wide SX cabinet with 19" mounting rails (AR3100 or AR3300) we offer sku AR7510. This is a set of four replacement 23" mounting rails, 42U.
  • We do not currently offer 48U 23" mounting rails as a stand alone sku, only pre-installed into the cabinet as described above.
  • We do not currently offer 45U 23" mounting rails. If you have an opportunity please check with your Schneider Electric representative to see if these can be provided as a Custom.
How to order a custom cabinet with 23" mounting rails installed: 
​If you buy direct from APC please contact your Sales Representative for price and availability. 
If you don't have an account with APC please contact APC Tech Support. We will give you a custom part number that can be quoted through a reseller or distributor. 

Compatibility Note: 23" wide mounting rails do not install into 600 mm (24") wide cabinets because the cabinets are not wide enough. 23" rackmount equipment requires a wider cabinet. 
Was this helpful?
What can we do to improve the information ?