Browse FAQs

Where can I find the Q2C or Factory Order number for an enclosed ATS48 soft start?

Published date: 19 July 2019

Issue:
Need to identify the Factory Order, or Quote to Cash number for an enclosed ATS48 soft start.

Product Line:
Enclosed Altistart 48, Enclosed ATS48, 863848U, 863948U

Environment:
All models

Cause:
To determine warranty status or check the Bill of Materials for spare parts.

Resolution:
Find the nameplate on the back of the enclosure door.  At the bottom of the nameplate on the right side is a box labeled Factory Order Number.  This should contain an 11 digit number which is the Factory Order / Q2C number.

Was this helpful?

What can we do to improve the information ?