Technical FAQs

Ask a Question

Are Schneider Electric Altivar drives 6, 9, 12, 18 or 24-pulse?

Issue:
Are Schneider Electric Altivar drives 6, 9, 12, 18 or 24-pulse?     

Product line: 
Altivar 61 71 12 312 212 320 32 630 650 930 950

Environment: 
All models, all serial numbers  

Cause:
None

Resolution:
Schneider Electric Altivar VFDs are 6-pulse.  The enclosed Power Guard is 18-pulse.
Was this helpful?
What can we do to improve the information ?