What is the difference between a standard ION6200 and ION6200 MW option?
Issue
Determining the difference between the standard and Megawatt versions of the ION6200
Product Line
ION6200
Environment
Using metering in a power monitoring application
Cause
Need measurement value with the proper scaling at the front display
Resolution
There are two main differences between the ION6200 and ION6200MW (megawatt option).
The Powerlogic® ION6200 Megawatt option displays all power and energy values in millions (e.g. megawatts) and volts in thousands (kilovolts), using a different front panel faceplate than the standard meter, with labels for kV, MW, MVA, MVAR, MWh, MVAh, and MVARh.
The PT Scaling setup register provides an additional PT primary register to accommodate a larger PT ratio. PTS offers a x1000 quantity for the PT primary register. The standard meter model uses the x1 default scaling.