Browse FAQs

What is the difference between a Micro 110CPU61200 and Micro 110CPU61204 controller?

Published date: 31 July 2019

Issue
Difference between PLC's

Product Line
Modicon Micro

Resolution
There are two main differences.
The Micro 110CPU61200 has 2K logic memory words.
The Micro 110CPU61204 has 8K logic memory words and Comm port 2 supports XMIT Block Modbus Master.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.