Browse FAQs

What are the different ways of connecting to the TSXETG1010 module for accessing data?

Published date: 14 August 2019

Issue: 
Different ways of connecting to the TSXETG1010 module for accessing data


Product Line:
TSXETG1010


Resolution:
There are 3 ways of accessing remote device data:
1. Directly, where the PC is connected directly to the module via the Ethernet
network.
2. Remotely, where the PC polls the module via the telephone network (via modem)
and can therefore acquire Uni-Telway device data.
3. By a combination of the two (direct and remote), where the PC is connected to
the module directly (via Ethernet) and remotely (via modem).

With any of these 3 connections, the user can access Uni-Telway device data, HTML pages, variable tables, animation tables, and screen pages.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.