Browse FAQs

On the ATV71 torque limitation, are the Motoring torque limit (tLIM) and Gen. torque limit (tLIG) values based on the torque rating of the motor or on the ratings of the drive?

Published date: 06 August 2019

Issue:
What is the torque rating based on?  On the ATV71 series, Motoring torque limit (tLIM) and General torque limit (tLIG) state that they can be adjusted between 0 and 300% of the rated torque.

Product Line:
ATV71

Environment:
All model and serial numbers

Cause:
None

Resolution:
The nominal torque is calculated in the drive on the basis of the motor parameters entered into the drive.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.