Browse FAQs

How to set up the basic PID control on the ATV61 or ATV71 drives?

Published date: 01 July 2019

Issue:
How can do you set up the PID control? on the ATV61 Drives?

Product line:
ATV61 and ATV71

Environment:
All models, all serial numbers

Cause:
PID set up to maintain pressure control with a fixed pressure set point

Resolution:
Application function menu 1.7
PID programming
PID regulator
PID feedback assign(PIF)= signal for the PID loop feedback
Min PID feedback(PIF1)= 0 example only
Min range of PID signal
Max PID feedback(PIF2)= 1000 example only
Max range of PID signal
Min PID reference(PIP1)= 100 example only
Min range of PID window
Max PID reference(PIP2)= 900 example only
Max range of PID window
Act. internal PID ref(PII)= Yes set point is from internal PID ref(rPI)
Internal PID set point
PID Prop. gain(rPG)= 0.75 example only
PID Loop response
PID integral gain(rIG)= 0.1 example only
PID Loop response
PID ramp(PrP)= 6 seconds example only
Auto/Manual Assign(PAU)
Switch to and from PID mode
Acceleration 2(AC2)= 5 seconds factory default
Acceleration before the VFD enters the PID window
Manual reference(PIn)
Speed reference when Auto/Manual assign(PAU) input is active  
ATV61_Programming manual

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.