Technical FAQs

Ask a Question

What level of control would I have over my KNX lighting system?

The interior and exterior lighting of a building can be switched or dimmed individually,in groups or from an unlimited number of locations.The operation is carried out manually via KNX push buttons,remote control via radio as well as automatically dependent on time, brightness and movement via automatic detection of people in the vicinity.
Lighting in a room which is switched and/or dimmed can be combined together in a scene mode format.The light scene can be modified ,stored and retrieved by the user at any time.
Was this helpful?
What can we do to improve the information ?